What is the SMA connector that is mounted repeatedly for test/evaluation ?

Modified on Fri, Jun 26 at 12:40 PM

There are several connectors that fixed on board(PCB) with screws not soldering. 
They eliminate the soldering influence on high frequency performance.
HRM(G)-300-467B-2: Edge (end) launch
HRM(G)-300-468B-2: Vertical launch
There are screw fixing connectors in SMA(-30G Hz), 2.92mm (-40G Hz),
2.4mm(-50G Hz,1.85mm(-65G Hz) ranges.