Is it possible to connect DF12N(DF17) series with the mate even if it is rotated 180 degrees horizontally ?

Modified on Fri, Jun 26 at 12:43 PM

As ​DF12N series is vertically & laterally symmetric on the mating side, they can mate with the mate even if it is rotated 180 degrees.
DF17 series has the same structure.