The mounting style for UX60SC-MB-5S8(80) is SMT according to Web site. However, there are through holes on PCB mounting pattern. Is the flow soldering used?

Modified on Fri, Jun 26 at 12:45 PM

The reflow soldering is used for SMT signal contacts and the lead reflow is used for metal shield. UX60SC-MB-5ST(80) is the connector that the reflow soldering is used for all contacts.