No, it can be used without any problems.
In case of screw type terminal block, it is a problem because the screw loosens when cable moves, but there is no problem in case of the zero screw terminal block because of spring type. The reliability test was done to confirm.
In case of screw type terminal block, it is a problem because the screw loosens when cable moves, but there is no problem in case of the zero screw terminal block because of spring type. The reliability test was done to confirm.